- No : 21572
- Release Date : 2018/08/22 16:28
-
Print
Harmonic suppression guidelines for power supply
How should I consider the harmonic suppression guidelines for power supply?
What is the circuit type?
- Category :
-
Answer
Since the high power factor converter uses the self-excitation three-phase bridge (voltage type PWM control) circuit configuration (type), the conversion coefficient is defined as K5 = 0 in the guidelines.
The conversion coefficient of 0 means that it does not generate harmonics. Therefore, it is not required to consider the high power factor converter as a harmonics generator.
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option