- No : 21578
- Release Date : 2018/08/22 16:28
-
Print
Can a single potentiometer operate two speed controller?
Can a single potentiometer operate two speed controller?
- Category :
-
Answer
A single potentiometer cannot operate two speed controller.
Reason:
Since the control circuit and main circuit of the SC-A speed controller are not insulated, connecting two speed controllers to a single potentiometer may generate undesirable current that may break the speed controllers.
(You can operate two speed controllers by using an insulated double potentiometer.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter speed controller
- Series
- SC-A