• No : 21616
  • Release Date : 2018/08/22 16:28
  • Print

How many inverters can I connect using the communication unit?

How many inverters can I connect when the communication unit (FR-CU01 or FR-CU03) is used?
Category : 

Answer

Since the communication unit conforms to the EIA Standard RS-485, up to 32 inverters can be connected. (Transmission format: Multidrop link, total wiring length: 500 m)(Note) Use the connection cable FR-CBL when using the FR-CU01.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024