- No : 21641
- Release Date : 2018/08/22 16:28
-
Print
Motor wiring length
How far apart can the vector inverter and motor be?
- Category :
-
Answer
Up to 50 m. Be sure to connect the encoder cables in parallel and use the thicker cable gauge.
You can extend this distance up to 100 m by using the long distance cable power supply that is a plug-in option.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200