• No : 21656
  • Release Date : 2018/08/22 16:28
  • Print

Plug-in options

Can I reuse the plug-in option for the FR-A200E?
Category : 

Answer

You cannot reuse the plug-in option for the FREQROL-A200 and A100 series.
You must use one of the following three plug-in options dedicated to the FREQROL-V200:
Note that these dedicated options cannot be used with the FREQROL-A100/A200 series.
- FR-VPA (additional I/O function)Additional input 6 points, additional analog input 1 pint, orientation control, additional output 3 points, long distance cable (50 m to 100 m) power supply, encoder pulse output (open collector)
- FR-VPB (position control function)Position control, additional analog input 1 point, RS485 interface, long distance cable (50 m to 100 m) power supply, encoder pulse output (line driver)
- FR-VPC (digital 12-bit input)Encoder pulse output (line driver, A and B only), long distance cable (50 m to 100 m) power supply, digital 12-bit input, motor thermistor interface, additional analog input 1 point
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
FR-V200