- No : 21835
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
By attaching the CC-Link optional card FR-A7NC E kit, how long does the depth of the inverter increase?
- Category :
-
Answer
By attaching the optional card and dedicated cover, the depth increases by approximately 15 mm for the FR-E700, and approximately 22 mm for the FR-E700-SC.
Since the terminal block protrudes from the front cover, the depth further increases by approximately 2 mm (2.8 mm at the maximum).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700