- No : 21923
- Release Date : 2018/08/22 16:30
-
Print
Operation at base frequency or higher
What the output frequency of the inverter is when the base frequency is set to 50 Hz and the setting frequency is set to 55 Hz?
The maximum frequency is set to 60 Hz.
- Category :
-
Answer
The output frequency is 55 Hz. (For V/F control)
When the base frequency is set to 50 Hz, frequencies over 50 Hz is the constant output range.
Note that the maximum torque during 55 Hz operation is lower than that of the 50 Hz operation.
- Product Name
- Inverter, magnet motor drive
- Series
- Others