- No : 21931
- Release Date : 2018/08/22 16:30
-
Print
400 Hz output setting
Which parameter should I change to change the output to 400 Hz?
- Category :
-
Answer
Change Pr.18 (High speed maximum frequency) to 400 Hz.
If you are using the analog command to set the frequency, calibrate the 400 Hz frequency with Pr.903.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500