- No : 21947
- Release Date : 2018/08/22 16:30
-
Print
Speed 15 operation
I must implement automatic control with 15 speeds using a standard 0.75 kW motor.
Which inverter should I use for this purpose?
When can I use the multi-speed command parameter?
Can I use it in my case where using 15 speeds is necessary?
Since the number of necessary speed ranges may exceed 15, I also must consider expandability.
- Category :
-
Answer
Using the inverter's input terminal, you can use up to 15 speeds.
This function is supported by the current 500 series products (A500, F500, E500, and S500).
Using analog input, terminal JOG (A500 and F500 only), adjustment frequency, you can add more speeds for some inverter types.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-S500, FR-E500, FR-F500, FR-A500