• No : 21953
  • Release Date : 2018/08/22 16:30
  • Print

Selection of high-duty brake resistor

I use a 5.5 kW motor with the FR-E520-7.5K, but the braking efficiency is not sufficient and I want to attach the high-duty brake resistor. Should I select the high-duty brake resistor according to the motor capacity or inverter capacity?
Category : 

Answer

Select the high-duty brake resistor according to the inverter capacity.
Product Name
Inverter, magnet motor drive
Series
FR-E500, FR-A500