- No : 21971
- Release Date : 2018/08/22 16:30
-
Print
Inverter 200 V input and 400 V output
I am considering to purchase a 45 kW or 55 kW inverter.
When using the inverter with 200 V input and 440 V output, is it common to use a 400 V class inverter by boosting the voltage on the input side of the inverter using a transformer?
Do you have any inverter that directly takes 200 V input and generates 440 V output?
- Category :
-
Answer
We do not have an inverter that directly takes 200 V input and generates 440 V output. Therefore, as you mention, use a 400 V class inverter by boosting the voltage on the input side of the inverter.
If the input is 200 V, you can also use a 200 V class inverter with a motor.
- Product Name
- Inverter, magnet motor drive
- Series
- Others