• No : 21973
  • Release Date : 2018/08/22 16:30
  • Print

External wiring for CC-Link operation

When connecting via CC-Link using the FR-A500 + FR-A5NC or FR-E520-□□KN (CC-Link type), is external wiring (for example, for the start command) necessary?
Category : 

Answer

For the combination of the FR-A500 + FR-A5NC, Pr.338 and Pr.339 are used to specify whether the external signals or CC-Link commands are used to set the running frequency and start the inverter. If you choose the external signals, you need external wiring.
Since the FR-E520-□□KN does not have a terminal for an external wire (for example, for the start signal), the CC-Link commands are used to start and stop the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500, FR-A500