- No : 21979
- Release Date : 2018/08/22 16:30
-
Print
Input power supply circuit breaker
For a circuit breaker attached to the input power supply of the inverter, while the Instruction Manual specifies MCCB and NV series only, can I use a motor circuit breaker?
- Category :
-
Answer
When using a motor circuit breaker, the rated current of the motor circuit breaker to use must be equal to or higher than the rated current of the circuit breaker mentioned in the inverter's the Instruction Manual and catalog.
- Product Name
- Inverter, magnet motor drive
- Series
- Others