- No : 21980
- Release Date : 2018/08/22 16:30
- 
          
              Print
          
        
 
Speed adjustment of multiple inverters using variable resistor
    
      Can I adjust the speed of multiple inverters using a single external variable resistor?
If I can, let me know how to connect them.
    
  
    - Category : 
- 
      
    
 
    Answer
  
    You can connect up to three inverters in parallel to an external variable resistor. Refer to the figure below for a connection example. By setting parameters (analog signal gain and bias), you can proportionally operate the inverters at different frequencies. Figure 1
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Series
- Others