• No : 21984
  • Release Date : 2018/08/22 16:30
  • Print

Changing parameters

Can I switch between the operation panel potentiometer and current input from an external source with the FR-E520 series inverter?
Category : 

Answer

Before you change Pr.7 and Pr.8, you must switch to the PU operation mode. Switch to the PU operation mode and change them.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F500