- No : 21993
 
      - Release Date : 2018/08/22 16:30
 
        - 
          
              Print
          
        
 
  
 
Deceleration overvoltage (E.OV3)
    
      I replaced the FR-Z220-2.2K inverter connected to a machine with the FR-E520-2.2K. The E.OV3 error occurred when the machine stops. I adjusted the deceleration time and other settings, but the error persisted. When I replaced the inverter with the original FR-Z220-2.2K, the error disappeared.
(The error did not occur at low speed (around 20 Hz), but occurred during automatic operation at 60 Hz.) What is the difference between the FR-E520 and Z/A series?
Do I have to change the inverter to the FR-A520 in such cases?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    While the FREQROL-Z200 series and A500 series have a brake resistor built in the capacity up to 7.5K, the FREQROL-E500 series does not have a built-in brake resistor.
Therefore, with FR-E520-2.2K, regenerative power cannot be handled at rapid deceleration and the E.OV3 error may occur.
To counteract such a case, you can attach an external brake resistor (not available for 0.2K or less). Attach the FR-ABR-2.2K.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-E500