- No : 22008
- Release Date : 2018/08/22 16:30
-
Print
Alarm output signal when using CC-Link
Among the signals sent from the FR-E520 inverter for CC-Link to the master unit, what is the difference between RX7 (fault) and RX1A (error status flag)?
- Category :
-
Answer
The RX7 output signal is the same as the signals for NO, NC, and transfer contact output.
You can change the contents of this output signal using Pr.192.
Pr.192 is initially set to "99" (fault output) and same as RX1A.
Since changing the setting of Pr.192 changes the output contents of RX7, RX1A is provided as a dedicated fault signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500