- No : 22027
- Release Date : 2018/08/22 16:30
-
Print
Two-rank up maximum short-time torque
While the maximum short-time torque is determined by the inverter capacity, what are the short-time torque coefficients for two-rank up and three-rank up combinations?
- Category :
-
Answer
It is not possible to generate torque larger than the maximum possible torque of the motor by increasing the inverter's capacity.
Even when the inverter is upgraded by two or three ranks, use the same torque coefficient as used for upgrading the inverter by one rank.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500