- No : 22065
- Release Date : 2018/08/22 16:30
-
Print
Reset command during operation
1. The following fault occurred:
(1) The parameter unit (FR-DU04) did not display anything.
(2) While the POWER on the side of the parameter unit and ALARM LEDs were turned on, the inverter input side power supply was turned off to reset the inverter, but the above situation persisted.
2. I checked the hardware circuit and found that a fault reset with other than the inverter also reset the inverter.
Is this circuit design related to the error?
- Category :
-
Answer
The reset signal does not damage the inverter.
It seems that the inverter went faulty due to other reasons.
Mitsubishi Electric FA Center can inspect the inverter to find out the cause. Contact your distributer or our local office.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500