- No : 22070
- Release Date : 2018/08/22 16:30
-
Print
Operation command terminal switching
While the FR-E520 is rotating in the forward direction with the terminal STF turned ON, how does the inverter operate if it is switched to STR (with STF turned OFF)?
- Category :
-
Answer
It rotates in the forward direction while STF is ON.
And then, when STR is turned ON and STF is turned OFF, the inverter decelerates down to 0 Hz within the specified deceleration time. Then, it accelerates to the setting frequency in the reverse rotation within the specified acceleration time.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500