- No : 22075
- Release Date : 2018/08/22 16:30
-
Print
Brake sequence function
I want to use the brake sequence function with a 0.1 kW motor.
The A500 series allows for using this function from 0.4 kW. Can I use this function with 0.1 kW by setting parameters?
If not, can I do this with another series of inverters?
- Category :
-
Answer
Since the brake sequence function requires Advanced magnetic flux vector control and advanced flux control is applied to 0.4 kW or higher motors, you cannot use the brake sequence function with a 0.1 kW motor.
No other series of inverters has the built-in brake sequence function.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500