- No : 22080
 
      - Release Date : 2018/08/22 16:30
 
        - 
          
              Print
          
        
 
  
 
Pulse frequency characteristics of terminal FM
    
      I want to display the frequency on a pulse input device such as a rotational HMI (Human Machine Interface).
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    The terminal FM output pulse is directly proportional to the inverter output frequency.
With the initial setting, 1440 pulses/sec are output at 60 Hz (Pr.55), and up to 2400 pulses/sec can be output.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Series
 
          - Others