• No : 22081
  • Release Date : 2018/08/22 16:30
  • Print

Which motors can I use with the inverter?

Let me know which types of motors I can use with the inverter.
Which should I choose from various types of motors (for example, geared motors, induction motors)?
Category : 

Answer

You can use general-purpose three-phase induction motors.
You can also use geared motors if the motor itself is an induction motor.
Synchronous motors are not recommended due to possible synchronization loss.
Note that single-phase motors cannot be used.
Product Name
Inverter, magnet motor drive
Series
Others