- No : 22084
- Release Date : 2018/08/22 16:30
-
Print
Can I drive multiple motors with a single inverter?
Can I drive two 0.4 kW motors and one 0.1 kW motor with a single inverter?
- Category :
-
Answer
You can drive multiple motors with a single inverter.
However, since the inverter cannot determine the current of each motor, the electronic thermal O/L relay cannot be used.
Therefore, you need to attach an external thermal for each motor for protection.
- Product Name
- Inverter, magnet motor drive
- Series
- Others