• No : 22085
  • Release Date : 2018/08/22 16:30
  • Print

Operation panel extension cable

The specifications of the extension cable for the operation panel of the inverter E500 are same as the 10BASE-T (straight) LAN cable used to connect a hub and personal computer. Is this correct?
Can I use this type of cable within the limit of 20 m?
Category : 

Answer

Yes, you can use the 10BASE-T cable (straight) with the E500.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500