• No : 22089
  • Release Date : 2018/08/22 16:30
  • Print

Inverter stop-on-contact control

I want to implement stop-on-contact control with the inverter.
I also want to connect the inverter and programmable controller via CC-Link.
Can I realize both of them simultaneously?
Category : 

Answer

Use the FREQROL-A500 series inverter with the optional FR-A5NC.
Then, you can implement both of stop-on-contact control and CC-Link operation.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500