- No : 22099
- Release Date : 2018/08/22 16:30
-
Print
Motor rated rotations per minute
Is it possible to use a standard three-phase motor (SF-JR) 2-pole 0.4 kW and the inverter to perform high-speed rotation of 4000 to 6000 (MAX 9000)?
- Category :
-
Answer
The inverter is capable of output up to the maximum frequency. It is the matter of whether the motor used support high-speed operation.
In the situation you mention, it is considered to be hard for the motor to operate at that high speed.
For details, consult our technical support below.
Shinshiro plant technical telephone support Phone: 0536-25-0900
- Product Name
- Inverter, magnet motor drive
- Series
- Others