- No : 22132
- Release Date : 2018/08/27 16:41
-
Print
As to using SD memory card at multiple locations.
As to measurements at several points using the EcoMonitorLight, is the number of SD memory card used for the Logging Unit needed for the number of the Logging Unit?
- Category :
-
Answer
Setting different logging ID enables that one SD memory card can be used for several Logging Units. Settable logging ID is 1 to 255.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight