- No : 22139
 
      - Release Date : 2018/08/27 16:41
 
        - 
          
              Print
          
        
 
  
 
As to changing location of the decimal point and units of the measured value.
    
      Is it possible to change location of the decimal point or units of the measured value displayed in the Operating mode?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Since location of the decimal point or units of the measured value displayed is decided by Total load power, it is impossible to change location of the decimal point or units separately. Check [Display of Measured item in the Operation mode] in user's manual detailed edition for the location of the decimal point or units displayed. 
The manual is downloaded in this site. 
* Total load power is calculated as below: 
Total load power(kW) = a x primary voltage(V) x primary current (A) / 1000
(a = Single-phase 2-wire system:1 Single-phase 3-wire system:2 Three-phase 3-wire system:√3 Three-phase 4-wire system:3)
  
    
      
        - Product Name
 
          - Energy Measuring Units
 
      
      
        - Series
 
          - EcoMonitorLight