- No : 22285
- Release Date : 2018/08/30 13:55
- 
          
              Print
          
        
 
Regarding the type of battery which can be used with the CPU module.
    
      What is the model name of the battery that can be used with the CPU module?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    FX3U-32BL can be used.                                                                                          
The battery is not included with the CPU module during factory shipment.
The battery can be used to increase the capacity of the latch device/label, as well as to maintain the clock data during power interruption.
  
    
      
        - Product Name
- FX5U, FX5UC
        - Product Category
- CPU Module, Options
        - Series
- MELSEC iQ-F Series