• No : 22287
  • Release Date : 2018/08/30 13:55
  • Update : 2023/07/03 11:56
  • Print

Regarding the processing specification of the basic operation instruction(LD).

What is the processing specification of the basic operation instruction(LD)?
Category : 

Answer

The execution time of the basic opeartion instruction (LD) of the FX5U/FX5UC/FX5UJ CPU module is 34 ns. *For firmware Ver.1.100 or above, this specification applies to 64K step mode.
The execution time of the basic opeartion instruction (LD) of the FX5S CPU module is 84 ns.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series