• No : 22298
  • Release Date : 2018/08/30 13:55
  • Update : 2023/02/14 09:53
  • Print

Regarding address change of positioning operation.

Can the positioning address be changed to an arbitrary value during the positioning operation?
Category : 

Answer

It can be changed.
For example, with the positioning instruction, a word device can be assigned to the operand which specifies the positioning address and the address can be changed by rewriting the value.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Motion/Positioning
Series
MELSEC iQ-F Series