• No : 22306
  • Release Date : 2018/08/30 13:55
  • Update : 2023/06/23 10:48
  • Print

Regarding CW/CCW(Forward pulse/Reverse pulse) output of the built-in positioning function

Does CPU built-in positioning function support CW/CCW(Forward pulse/Reverse pulse) output?
Category : 

Answer

FX5U/FX5UC/FX5S CPU modules are supported. Up to 2 axes are available in GX Works3 parameter settings.
In addition, up to 8 axes can be added by adding a high-speed pulse I/O module.
The built-in positioning function of the FX5UJ CPU module does not support CW/CCW output. Up to 8 axes can be added by adding a high-speed pulse I/O module.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Motion/Positioning
Series
MELSEC iQ-F Series