• No : 22308
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the link refresh settings of FX5-CCL-MS

When setting the link refresh settings from GX Works3 by configuring the CC-Link module FX5-CCL-MS as a master station,
is it possible to check the device assignment settings of the refresh devices?
Category : 

Answer

By selecting the appropriate module number from the option "Mount Position Number No." accessed from [View]→[Docking Window]→[Device Assignment Confirmation] of GX Works3 menu, the allocated number can be checked.
However, the link refresh settings from the parameter settings of CC-Link must be set in advance.
Product Name
FX5-CCL-MS
Product Category
CPU Module, Network/Communication, Engineering Software, GX Works3
Series
FX5U,FX5UC