• No : 22312
  • Release Date : 2018/08/30 13:55
  • Update : 2022/12/22 10:18
  • Print

Regarding the frequency of high-speed counters

Answer

The maximum frequency of the FX5U/FX5UC CPU module is 200kHz and the maximum frequency of the FX5S/FX5UJ CPU module is 100 kHz.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, High-Speed Counter
Series
MELSEC iQ-F Series