• No : 22314
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the settings of built-in analog function of FX5U CPU module

Are there any required settings for using the built-in analog function?
Category : 

Answer

The settings can be done using the parameter settings of GX Works3 or by settings the special relay/special registers.
For further details please refer to MELSEC iQ-F FX5 User's Manual (CPU Module Built-In Analog/Expansion-Adapter).
6 FX5U CPU MODULE BUILT-IN ANALOG
6.7 Parameter Setting
Product Name
FX5U
Product Category
CPU Module, Analog Control
Series
FX5U