• No : 22317
  • Release Date : 2018/08/30 13:55
  • Print

Regarding setting CC-Link settings using GX Works3

Answer

Parameters can be set when connecting the MELSEC iQ-F series with FX5-CCL-MS(CC-Link system master/intelligent device).
However, when connecting with FX3U-16CCL-M(CC-Link master), the settings must be configured using a program.
For further details, please refer to the example programs in FX3U-16CCL-M User's Manual.
12.1.3 Setting of parameters
1. Program for parameters
Product Name
FX3U-16CCL-M, FX5-CCL-MS
Product Category
CPU Module, Network/Communication, Engineering Software, GX Works3
Series
FX5U,FX5UC