• No : 22323
  • Release Date : 2018/08/30 13:55
  • Print

Regarding expansion of communication ports

Is is possible to add communication port to FX5U/FX5UC CPU module and use the MODBUS communication on multiple communication channels?
Category : 

Answer

It is possible to use the MODBUS serial communication with multiple channels.
However, only 1 channel can be set as the master.
The MODBUS serial communication settings can be set from GX Works3 parameters.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series