- No : 22323
- Release Date : 2018/08/30 13:55
-
Print
Regarding expansion of communication ports
Is is possible to add communication port to FX5U/FX5UC CPU module and use the MODBUS communication on multiple communication channels?
- Category :
-
Answer
It is possible to use the MODBUS serial communication with multiple channels.
However, only 1 channel can be set as the master.
The MODBUS serial communication settings can be set from GX Works3 parameters.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series