• No : 22329
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the latch settings of data register

When FX5U/FX5UC CPU module's power is set to OFF, data register(D100) is cleared.
Are there any settings required to latch this register?
Category : 

Answer

It is necessary to set the latch range from the following GX Works3 parameters:
[Navigation Window] -> [CPU Parameters] -> [Device/Memory Settings] -> [Device/Label Memory Area Setting]
Product Name
FX5U, FX5UC
Product Category
CPU Module, Engineering Software, GX Works3
Series
MELSEC iQ-F Series