- No : 22368
- Release Date : 2018/08/31 14:33
-
Print
Trip button
What is Trip button ?
- Category :
-
Answer
It is a button in order to mechanically trip a circuit breaker outside. It is used to confirm switching mechanism at the regular maintenance or sequence-check when installing Alarm switch (AL). NOTE: In some models, there is no trip button. Moreover, Some models does not trip at "OFF" state. The trip button has red color and installed on the front of circuit breaker. This is also called as PTT (Push To Trip).
- Product Name
- Molded Case Circuit Breakers
- Series
- WS-V