- No : 22397
- Release Date : 2018/08/31 14:33
-
Print
How to use TBM
What is TBM (Test Button Module)?
- Category :
-
Answer
It is an internal accessory to test the earth leakage tripping operation by applying voltage remotely. It is possible to make the same control sequence as the SHT of MCCB, and parallel connection of the TBMs is also possible. (While applying the control input voltage, it remains the state as pushing test button) General TBM includes SLT(vertical lead wire terminal block)
- Product Name
- Internal Accessories
- Series
- WS-V