- No : 22400
- Release Date : 2018/08/31 14:33
-
Print
Side by side installation
Is it possible that MCCBs or ELCBs are closely installed?
- Category :
-
Answer
It is possible to attach closely if there is no problem about the insulation distance between live parts such as a terminal bar and load currents are 80% or less than the rated current.
- Product Name
- Molded Case Circuit Breakers
- Series
- WS-V