• No : 22406
  • Release Date : 2018/08/31 14:33
  • Print

Insulating barrier in the package

Is it necessary to use the insulating barrier that is included in the package?
Category : 

Answer

Use the insulation barrier if they are packed with. If not using that, breaking performance is not guaranteed. For models that the insulation barrier is not included in the package, there is no problem when connecting the wires specified in the standard. However, please use barrier if insulation distance is insufficient when connecting a thick cable.
Product Name
External Accessories
Series
WS-V