• No : 22425
  • Release Date : 2018/08/31 14:33
  • Print

ACB reverse connection

Is it possible to use line side and load side connected in reverse?
Category : 

Answer

For ACB, Line and Load are not defined on the main circuit terminals. Reverse connection is available without any limitation.
Product Name
Low Voltage Air Circuit Breakers
Series
WS-V