- No : 22438
- Release Date : 2018/08/31 14:33
-
Print
Default setting of electronic breakers
What is the default set value of an overcurrent characteristic setting knob of an electronic circuit breaker when shipping?
- Category :
-
Answer
Each setting knob of the overcurrent trip characteristic is set to the maximum value and then shipped if not specified. However, only the pre-alarm is set to the minimum value (70%).
- Product Name
- Molded Case Circuit Breakers
- Series
- WS-V