• No : 22443
  • Release Date : 2018/08/31 14:33
  • Print

Degree of protection

What does "degree of protection" mean?
Category : 

Answer

In order to prevent breakdowns and human injuries, it is necessary to select a control device having protection structure suitable for each purpose. The protection class of the control devices is called "degree of protection". This can be classified depending on the structure for human body and protection against water intrusion etc.
Product Name
Molded Case Circuit Breakers
Series
WS-V