• No : 22459
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/18 15:24
  • Print

How to establish the USB communication between GX Works3 and a CPU module

How can I establish the USB communication between GX Works3 and a CPU module?
Category : 

Answer

To establish the USB communication with a CPU module, install a USB driver.
The following describes the installation procedure.
When multiple MELSOFT applications have been installed, install a USB driver as follows.

(a) When GX Developer has been installed first
      Specify "C:\MELSEC\Easysocket\USBdrivers".
(b) When GX Works2 has been installed first
      Specify "C:\Program Files\MELSOFT\EasySocket\USBDrivers".
(c) When the "USBDrivers" folder does not exist in the above folders (a) and (b)
      Search for the "USBDrivers" folder in File Explorer and check the location of the folder.



For details, refer to the following manual.
- GX Works3 Operating Manual Appendix 6 USB Driver Installation Procedure
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series