• No : 22487
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 09:37
  • Print

I cannot place a main base unit in a module configuration diagram with GX Works3.

I cannot place a main base unit in a module configuration diagram with GX Works3.
Category : 

Answer

You may have already placed a main base unit in the module configuration diagram.
Scroll up or down in the module configuration diagram and check if a main base unit has been placed in it.
When it has already been placed, you can place a new main base unit after deleting the existing main base unit.
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series