• No : 22490
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 09:46
  • Print

Interrupt period setting of fixed scan interrupts of MELSEC iQ-R series

How can I configure the interrupt period setting of fixed scan interrupts of MELSEC iQ-R series?
Category : 

Answer

You can configure the setting in "Interrupt Setting from Internal Timer" of the CPU parameter.

<Interrupt period setting>
[Navigation Window] -> [Parameter] -> [CPU Module] -> [CPU Parameter] -> [Interrupt Setting]
 -> [Fixed Scan Interval Setting] -> [Interrupt Setting from Internal Timer]
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series